串口0通讯默认位置1,P0_2和P0_3,DMA方式,参考这个我修改了协议栈配置部分代码,始终不能通过P1_4和P1_5即位置2来通讯,不知道哪里出了问题,导致配置始终不行,发出来大家帮看下:
定义HAL_UART=TRUE,修改 _hal_uart_dma.c文件里的相关参数将HAL_UART_DMA == 1里的地方都对应到uart0 lot2有如下
#if (HAL_UART_DMA == 1)
/*
#define PxOUT P0
#define PxIN P0
#define PxDIR P0DIR
#define PxSEL P0SEL
#define UxCSR U0CSR
#define UxUCR U0UCR
#define UxDBUF U0DBUF
#define UxBAUD U0BAUD
#define UxGCR U0GCR
#define URXxIE URX0IE
#define URXxIF URX0IF
#define UTXxIE UTX0IE
#define UTXxIF UTX0IF
*/
#define PxOUT P1
#define PxIN P1
#define PxDIR P1DIR
#define PxSEL P1SEL
#define UxCSR U0CSR
#define UxUCR U0UCR
#define UxDBUF U0DBUF
#define UxBAUD U0BAUD
#define UxGCR U0GCR
#define URXxIE URX0IE
#define URXxIF URX0IF
#define UTXxIE UTX0IE
#define UTXxIF UTX0IF
#if (HAL_UART_DMA == 1)
/*
#define HAL_UART_PERCFG_BIT 0x01 // USART0 on P0, Alt-1; so clear this bit.
#define HAL_UART_Px_RX_TX 0x0C // Peripheral I/O Select for Rx/Tx.
#define HAL_UART_Px_RTS 0x20 // Peripheral I/O Select for RTS.
#define HAL_UART_Px_CTS 0x10 // Peripheral I/O Select for CTS.
*/
#define HAL_UART_PERCFG_BIT 0x01 // USART0 on P0, Alt-1; so clear this bit.
#define HAL_UART_Px_RX_TX 0x30 // Peripheral I/O Select for Rx/Tx.
#define HAL_UART_Px_RTS 0x08 // Peripheral I/O Select for RTS.
#define HAL_UART_Px_CTS 0x04 // Peripheral I/O Select for CTS.
static void HalUARTInitDMA(void)
{
halDMADesc_t *ch;
P2DIR |= HAL_UART_PRIPO;
//PERCFG &= ~HAL_UART_PERCFG_BIT; // Set UART0 I/O to Alt. 1 location on P0.
PERCFG |= HAL_UART_PERCFG_BIT; // Set UART1 I/O to Alt. 2 location on P1.
uartConfig.configured = TRUE;
uartConfig.baudRate = HAL_UART_BR_115200;
uartConfig.flowControl = FALSE;
uartConfig.flowControlThreshold = MT_UART_THRESHOLD;
uartConfig.rx.maxBufSize = MT_UART_RX_BUFF_MAX ;
uartConfig.tx.maxBufSize = MT_UART_TX_BUFF_MAX ;
uartConfig.idleTimeout = MT_UART_IDLE_TIMEOUT;
uartConfig.intEnable = TRUE;
uartConfig.callBackFunc = smd_UartProcessData;
HalUARTOpen (HAL_UART_PORT_0, &uartConfig);