This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack 3.0.0的项目IAR 8051 8.20.2打不开

Other Parts Discussed in Thread: CC2530, CC2538

你好, 我们有一个ZigBee+以太网的项目,准备使用CC2530+以太网MAC来实现,CC2530主要是作为主机自动和ZigBee传感器组网,并将各传感器的数据通过串口发送到以太网Mac.

现在我们下载了Z-Stack3.0.0, 但是里面的projects下的所有项目都打不开,IAR提示的错误是:

查看过Z-Stack3.0.0需要的是IAR 8051 8.1.1以上,我们的是IAR 8051 8.20.2.

使用我们的IAR 8051打开BLE-CC254x-1.4.0没有问题.

请帮忙看看是什么问题, 怎样解决?

  •  Application, library, and hex files were built/tested with the following versions of IAR tools and may not work with different IAR tool versions:   - CC2538 + SRF06EB:  EWARM  7.70.1  (7.70.1.11486)   - CC2530 + SRF05EB:  EW8051 9.30.1 (9.30.1)

    版本偏低了

  •  安装9.30后是可以正常编译了.

    但是还是要吐槽下: TI是卖器件的,不是卖编译器的,能不能提供一些低版本的lib文件给大家.

    在8.20中手工建立项目后可以正常编译,但是不能链接,提示XLINK错误. 估计是你们提供的libraries下面的.a文件太新.