This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

连续调用AF_DataRequest发送函数,并没有按照规定的次数发送,这是什么原因?

尊敬的TI工程师以及在这方面有过研究的好朋友们:

        你们好,我现在需要连续50次发送一个数组uint8 Text[2] = {1,2},在协调器端用串口接收到发现只有6次,有时候也出现5次,每次调用的时候加了延时,效果还

是一样,单步调试,变量也再按部就班地改变,没有发现问题,可是在协调器那段只能接收到5-6次,没有开启低功耗。请您帮我分析下什么原因?下面是我的程序代

码。

 if ( events & GENERICAPP_SEND_VIB_EVT )

 {  uint8 Text[2]={1,2};

        for(uint8 m=0;m<50;m++)
{
        AF_DataRequest( &GenericApp_DstAddr, &GenericApp_epDesc,
        GENERICAPP_SEND_VIB,
        sizeof(Text),
         (byte *)Text,
         &GenericApp_TransID,
           AF_DISCV_ROUTE, AF_DEFAULT_RADIUS );


         Delay(100);
}

         return (events ^ GENERICAPP_SEND_VIB_EVT);

}

协调器接收数据的代码如下:

static void GenericApp_MessageMSGCB( afIncomingMSGPacket_t *pkt )
{
switch ( pkt->clusterId )
{
case GENERICAPP_SEND_VIB:


HalUARTWrite(0, pkt->cmd.Data, pkt->cmd.DataLength);                    //将振动发送函数发送的数据写到串口上

break;
}
}

请您帮我看看,哪里出现了问题?谢谢您