Other Parts Discussed in Thread: CC2530, CC2511
TI工程师们,请教一下以下问题:
问题一:CC2530外挂flash时,最大还能再挂多大的flash?
问题二:smartrf05eb,是不是已经外挂flash了?多大的?(从官网找到的原理图,好像已经外挂了,想确认一下)
问题三:如果硬件使用官网购买的smartrf05eb,软件使用HA协议栈中带OTA功能的sample,是不是就不用再修改软件底层了。
期待您的解答~~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
还有一个情况,我纠结了很久。ZigBee的开发板都是两块一起卖的。能不能买一个smartRF05 ,一个smartRF06。因为2530 2538各有长短,都想学,但是买两套板,实在太贵了。
还有个问题:关于管脚flash SPI引脚的连接关系
我看到smartRF05eb的原理图上,flash芯片 的SPI引脚,除了连接到2530的SPI 引脚外,还连接到CC2511。
目前我们没有外接flash,烧录治具一直用CCdebugger(就是DD/DC引脚)。如果外接FALSH,还能用原来的CCdebugger烧录治具吗?