This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530的OTA升级使用片内的flash够用么?

       (1)  如果使用的ZStack-CC2530-2.5.1a 协议栈 的OTA例程,cc2530 (256KB) OTA片内flash够用么;

        (2)使用的工程生成的镜像文件如附件所示:

         (3)生成的map信息:         

                 128 992 bytes of CODE memory (+ 131 012 range fill )
                 32 bytes of DATA memory (+ 75 absolute )
                 5 469 bytes of XDATA memory
                192 bytes of IDATA memory
                8 bits of BIT memory
                436 bytes of CONST memory