ZStack-1.4.3-1.2.1这个版本编译soft_start即可实现该功能,为什么后面的版本不支持了?现在使用zstark-2.5.1a,没有找到该功能如何实现。发现协调器在扫网后,如果空间内具有相同id的网络,则自动把panid+1后建网,尝试在这里改变器件角色,重新发起ZDOInitDevice,但是程序不能进入ZDO_NetworkDiscoveryConfirmCB(),求解答
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
ZStack-1.4.3-1.2.1这个版本编译soft_start即可实现该功能,为什么后面的版本不支持了?现在使用zstark-2.5.1a,没有找到该功能如何实现。发现协调器在扫网后,如果空间内具有相同id的网络,则自动把panid+1后建网,尝试在这里改变器件角色,重新发起ZDOInitDevice,但是程序不能进入ZDO_NetworkDiscoveryConfirmCB(),求解答
ZStack-1.4.3-1.2.1这个版本的说明文件里,还有这样一句话,It is possible to create an image with both Coordinator and Router functionality and choose the device type at runtime. See the SOFT_START compile option for more details.
但是后面版本的同一位置就没有这句话了,这个功能是被删掉了,还是可以通过其他的方式实现呢?