请问SRC_RTG_EXPIRY_TIME设置为多少合适??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个是源路由的timeout时间。首先请参考下面文档中,对这个变量的解释。
http://www.ti.com/lit/an/swra427c/swra427c.pdf
在2.2的最后一段,
If the concentrator is memory constraint, it is very important to note the source route expiry timeout (SRC_RTG_EXPIRY_TIME) value should be such that no more than (MAX_RTC_SRC_ENTRIES) devices reporting within this interval. In this case concentrator should be able to store the paths back to all the nodes as they report data (even if the concentrator does not have memory to store path to all devices) as expired routes will be replaced with new routes and the network should not see broadcast route request storms originating from the concentrator which can cause the network throughput and reliability to go down significantly.