Other Parts Discussed in Thread: Z-STACK
大家好:
我在《ZIGBEE SPECIFICATION 》(053474r20 )的以下章节:2.2.8.2.1 Binding Table Implementation
(as, es, cs) = {(ad1|, ed1|), (ad2|, ed2|) … (adn|, edn |)}
看到绑定entry的格式应该是一条cluster ID对应一条entry的。
但是在Z-stack的BindingTable.h BindingTable.c中绑定entry的结构体格式却是如下:
typedef struct
{
uint8 srcEP;
uint8 dstGroupMode; // Destination address type; 0 - Normal address index, 1 - Group address
uint16 dstIdx; // This field is used in both modes (group and non-group) to save NV and RAM space
uint8 dstEP;
uint8 numClusterIds;
uint16 clusterIdList[MAX_BINDING_CLUSTER_IDS];
} BindingEntry_t;
一条entry里面怎么可以有多个cluster ID呢?