This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-Stack Home 1.2.2a zgChildAgingEnable使能后, 发Orphan notification包, 原来是Data Request。

Other Parts Discussed in Thread: Z-STACK

请教TI的工程师, 通过抓包软件,发现 zgChildAgingEnable使能后, 现在都是Orphan notification,  原来是Data request。

孤儿通知

这种情况有问题吗?

  • 有帖子说是正常的?

    zgChildAgingEnable使能后, DPOLL_RATE=6000  DREJOIN_POLL_RATE=5000,  但是通过抓包软件, 发现每3s 终端就发出一个 Orphan notification。 

    这是哪里有问题吗? 我截取了两张图。

      (改变的数值为 timeoutCounter)

  • 1.2.2a的协议栈提供了两种aging 的方法,一种是发orphan 一种是发data request。 取决于父节点上zgNwkParentInformation 的取值

    zgNwkParentInformation = NWK_PARENT_INFO_MAC_DATA_POLL   使用 data request

    zgNwkParentInformation = NWK_PARENT_INFO_ORPHAN_NOTIFICATION; 使用 orphan notification

    默认使用orphan notification

    在ZGlobals.c 中 有一段代码 注释,上面讲得很详细:

    //=======    Child Aging PARENT ROUTER (ZR/ZC) configuration   ========
    // You can setup a router to support Child Table Aging in 1 of 2 modes of
    // operation.  The first mode is NWK_PARENT_INFO_ORPHAN_NOTIFICATION and it
    // expects end devices to use orphan scan periodically as a means of a keep-alive
    // notification to the parent.  The other mode is NWK_PARENT_INFO_MAC_DATA_POLL
    // which uses the end device's MAC POLL request as the keep-alive notification.
    // The first method is preferred for new devices, where the end devices provide
    // support for it (which will be manditory in future Zigbee Home Automation
    // Specifications).
    // The second method is compatible with older end devices without the need for
    // specific child aging support.
    //
    // The method supported by the router (or coordinator) is determined at build time
    // by setting zgNwkParentInformation to either NWK_PARENT_INFO_ORPHAN_NOTIFICATION
    // or NWK_PARENT_INFO_MAC_DATA_POLL.
    //
    // End device built with Child Table Aging support both methods, the method is
    // determined by the parent and communicated at run-time.

  • Hi,楼主

    您的 zigbee3.0入网成功了吗?

  • 请教一下, zgChildAgingEnable使能后, Orphan notification发送周期 不为 POLL_RATE, 这是什么原因了?

  • 暂时没用 z-stack 3.0了。

  • Orphan notification发送周期 不为 POLL_RATE????  这个倒没深入了解过!

    不知道VV 大神在不在,问问它!!!

  • @VV zgChildAgingEnable使能后, Orphan notification发送周期 不为 POLL_RATE, 这是什么原因了?

  • 如果是用orphan Notification来做keep alive的消息的话,那么周期是按照orphan scan的周期来的,跟poll rate没有关系。

    如果使用data request来做keep alive的话,那么就跟poll rate有关系

    建议使用data request来做keep alive

  • orphan scan 的周期是在哪里设置的???

    orphan scan 不是在断网的时候才发送吗? 它怎么会有周期呢???