Other Parts Discussed in Thread: CC2530
1.CC2530的内部基准电压是多少?我看到其他帖子里面技术支持说的是1.25V,但是使用1.25V比使用1.15V的误差还要大
2.使用1.15V做为基准电压测量VDD/3,最后的误差平均都有0.1V左右。想请问各位大神这个问题到底怎么处理,由于是电池设备所有只能有内部基准电压。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: CC2530
1.CC2530的内部基准电压是多少?我看到其他帖子里面技术支持说的是1.25V,但是使用1.25V比使用1.15V的误差还要大
2.使用1.15V做为基准电压测量VDD/3,最后的误差平均都有0.1V左右。想请问各位大神这个问题到底怎么处理,由于是电池设备所有只能有内部基准电压。
你好,请问如果以外部P07引入外部基准源为参考电压进行单次采集时,程序与以内部基准源为参考电压相比除了修改ADCCON3.EREF外还需要修改哪里?下边是我的程序,我以3012为基准源,同时基准源输出对外供电,但是发现基准源输出会出现抖动,一下是我的程序,请教
P0DIR &= ~0x02; // 设置P0.1为输入方式
APCFG |=0x02;
asm("NOP");asm("NOP");
/* Clear ADC interrupt flag */
ADCIF = 0;
ADCCON3 = 0X71;
/* Wait for the conversion to finish */
while ( !ADCIF );
asm("NOP");asm("NOP");
/* Read the result */
voltage = ADCL;
voltage |= (uint16_t)(ADCH << 8);
voltage >>= 4;
adc = voltage;