Other Parts Discussed in Thread: CC2530, CC2591, CC2590
指标:一是可增加CC2530的灵敏度6dB,二是有11dB的增益。
能否这样理解:增加CC2591,可以提高17个dB的接收性能?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不是哦。
主要是CC2590, cc2591的LNA的噪声系数好于芯片的,于是提高了接收机的解调信噪比,也就是灵敏度变好了3dB.这个是有效的。
当然了,改善了噪声系数,一定要有增益才可以改善整机接收噪声系数的。
BR. AZ