This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于默认信道问题

在协议栈中

一、f8wConfig.cfg中定义了:

-DDEFAULT_CHANLIST=0x02000000  // 25 - 0x19         //目前使用本信道号

二、MAC/Low Level/System/mac_radio_defs.h中定义了:

#define MAC_RADIO_CHANNEL_DEFAULT               11/* 11信道 */

请问:

一、这2个定义是否有冲突?

二、它们各有什么作用?

三、协调器在启动后,到底使用了哪一个信道呢?

  • f8wConfig.cfg中中定义的多了:

    //-DMAX_CHANNELS_868MHZ 0x00000001
    //-DMAX_CHANNELS_915MHZ 0x000007FE
    //-DMAX_CHANNELS_24GHZ 0x07FFF800
    //-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
    //-DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19
    //-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
    //-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
    //-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
    //-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
    //-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
    //-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
    //-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
    //-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
    //-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
    //-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
    //-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
    //-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
    //-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
    -DDEFAULT_CHANLIST=0x00000800 // 11 - 0x0B   这里默认的是11信道,跟MAC的定义没有冲突

  • 如果改为:

    //-DMAX_CHANNELS_868MHZ 0x00000001
    //-DMAX_CHANNELS_915MHZ 0x000007FE
    //-DMAX_CHANNELS_24GHZ 0x07FFF800
    //-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
    -DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19    默认的是25信道
    //-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
    //-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
    //-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
    //-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
    //-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
    //-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
    //-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
    //-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
    //-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
    //-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
    //-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
    //-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
    //-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
    //-DDEFAULT_CHANLIST=0x00000800 // 11 - 0x0B

    而MA层的定义不变,会和MAC的定义冲突吗?

  • 如果-DDEFAULT_CHANLIST没有定义,就用MAC_RADIO_CHANNEL_DEFAULT

    否则就用DEFAULT_CHANLIST定义的信道。