This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

z-stack 3.0.1 IAR FOR ARM 版本问题

Other Parts Discussed in Thread: Z-STACK, CC2538, CC2531, CC2530

我用的IAR 是7.80.3版本的。

打开最新下载的z-stack 3.0.1demo时,提示demo是由更高版本的IAR建的工程,当前版本打不开。

但是,打开z-stack 3.0.1的document 《Z-Stack 3.0 Sample Application User's Guide》在2.1 Required Software Tools章节中,提示:

EWARM version 7.70.1.11486 (for CC2538)


所以,有点懵。希望有成功打开demo的大神们,给个提示。

  • Z-Stack 3.0.1 is now available to download on TI.com at the link below. This SDK is a mainly a maintenance release for Z-Stack 3.0.0, no major new features were added but many bug fixes have been included. Full changes are available in the release notes included with the SDK. Since there were no major changes, migrating from Z-Stack 3.0.0 to 3.0.1 should be as simple as moving your IAR project files (for example, your SampleLight project folder) from the old SDK to the new SDK.

    Note that the IAR workspaces in this release have been updated to use the newest versions of IAR IDE, so you will need to make sure you are using the latest IAR IDE versions. The version numbers for IAR ARM and 8051 are available in the Z-Stack 3.0.1 release notes.

  • http://www.ti.com/tool/Z-Stack?keyMatch=z-stack&tisearch=Search-EN-Everything

    Application, library, and hex files were built/tested with the following versions of IAR tools. We recommend using the same IAR tool version

    • EWARM 8.11.1 (8.11.1.13272) for CC2538 Wireless MCU
    • EW8051 10.10.1 (10.10.1) for CC2530 and CC2531 Wireless MCU

    Please contact your local IAR office for further details on license purchasing.