Other Parts Discussed in Thread: Z-STACK, CC2530
协议栈:Z-Stack Home 1.2.2s
CPU:CC2530
测试节点:1个协调器,1个终端
测试环境:两个设备供电正常,距离2-3米,正常工作时通讯良好
终端节点程序修改及配置:
1.开启低功耗
2.每2s钟发送一次data Request
3.开启CHILD_AGING功能
4.按照VV大神建议,
if ( devStartMode == MODE_REJOIN )
{
_tmpRejoinState = true;
}
5.曾发现过 startMode为MODE_REJOIN,而_NIB.nwkState为NWK_ENDDEVICE 的状态机错误情况,因此
在ZDObject.c的ZDO_StartDevice()中,增加:#include "OnBoard.h"if ( ret != ZSuccess ){+ if( ret == ZNwkInvalidRequest ){ // 状态机出现错误+ SystemResetSoft(); //复位,重新加入网络+ }osal_start_timerEx(ZDAppTaskID, ZDO_NETWORK_INIT, NWK_RETRY_DELAY );}故障描述:1.通过抓包发现,终端设备运行一段时间后(几小时-几天)会出现停止发送data request及任何信息(无离网,重加网等任何信息),且设备无法进入低功耗状态(电池电压快速下降)。2.发现问题后,在应用层增加“每10分钟主动复位”的定时任务,没有再出现该问题,初步判断网络层运行异常,而应用层运行良好。请问:1.应用层有没有方法判断最近一次data request是否正常发送?这样在问题出现时才复位,而不是定时复位,降低复位功耗2.有无根本上解决这个问题的方法?谢谢