This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZSTACK 3.0.0 协调器始终保持再DEV_INIT状态

Other Parts Discussed in Thread: Z-STACK

使用协议是ZSTACK 3.0.0 版本,协议栈软件是从TI官方下载,没做啥修改,就加个串口打印联网状态,电路板用2.5.1的协议栈一点问题没有,程序也是官网的下载的,同样都是官网下载的程序,咋就组不起网呢,求大神指点

芯片使用的是CC2530F256,板子就接个串口,没其他东西

  • z-stack 3.0的协议栈默认是需要通过开发对应的按键进行菜单选择才能触发组网的。

    如果你需要上电就执行组网的话,可以调用下面的函数。

    如果你希望设备在上电以后,自动发起加网的话,你可以在初始化的地方加一个timer,设置1s,

    然后在timer事件处理的地方,调用bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_STEERING);