This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【求解】zstackHome1.22a里面的2630例程,怎么设置来生成hex文件?

刚接触zstack,打算用XDS100v3下载

  • 你用的什么编译器,IAR,CCS?都能生成hex文件

  • 用iar for arm7.4改设置之后可以出了。我看到社区别的前辈写的东西有一些不清楚的地方。还望指点一下。

    1,zstack core 相当于zstackHome系列的内核协议栈所以是公用的。这个内核工程通过在osal_run_system()中不断轮询tasksEvents[]来选取有事件标志中最高优先级的任务的loop函数来执行对吧。那是通过什么样的路径来和sampleDoorLock工程中的用户C文件中的函数关联起来的?

    2,比如我想使用2630的uart,在更改引脚定义后,调用uart_init(),uart_open(),然后在用户函数中可以正常使用吗?还是说需要另外去配置引脚的功能映射?