内容如标题
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那就是不包含咯,为什么ZigBee标准文档中说neighbor table包含
2.7.1.3.4 Neighbor tables
The neighbor table of a device shall contain information on every device within transmission range up to
some implementation-dependent limit. The information in stored in the neighbor table is used for a variety
of purposes, however, not all fields described in this subsection are required for the operation of a ZigBee
device. Each entry in the table shall contain the following information about a neighboring device:
— PAN identifier
— Extended address if device is parent or child
— Network address
— Device type
— Relationship