CC1101中的AGC功能可以关闭嘛,看到有三个AGC控制的寄存器,但是数据手册上没有解释,看不懂。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
比如你可以能在如下程序中看到用处:
CCA初始化函数如下:
void CC1101CCA( void )//配置为载波监听功能
{
CC1101WriteReg(CC1101_IOCFG2,0x0E);//GDO2引脚输出载波感应电平,如果RSSI级别在门限之上为高电平
CC1101WriteReg(CC1101_MCSM1,0x3F);//接受信号强度低于门限值且当前未接收报文则信道空闲,让TX和RX结束后,芯片都保持在RX状态。
CC1101WriteReg(CC1101_AGCCTRL1,0x40);//低噪声放大器增益先减小,载波监听相对阈值禁用,载波监听绝对阈值由MAGN_TARGET设置
CC1101WriteReg(CC1101_AGCCTRL2,0x07);//42dB
}
在手册搜索关键词应该可以看到。或者在头文件搜,也可以看到注释。