This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于z-stack 添加I2C功能的问题

Other Parts Discussed in Thread: Z-STACK, CC2538, CC2530, CC2538-SW

各位好,

应用有新需求,最近需在新项目上添加EEPROM用于扩展数据存储。

我从官网上下载了remote TI,并从中移植了I2C的驱动至Z-stack,具体如下:

在协议栈的HAL下添加了 hal_i2c.h和hal_i2c.c两个文件

然后在初始化中添加了

void HalDriverInit (void)
{
/*I2C*/
HalI2CInit(); //sfei 20171012


/* TIMER */
#if (defined HAL_TIMER) && (HAL_TIMER == TRUE)
#error "The hal timer driver module is removed."
#endif

…………

最后就是在应用中调用读写函数:

case 0xCC:
HalUARTWrite ( HAL_UART_PORT_0, I2Cdata, 3 );
HalI2CSend(0x52,I2Cdata+2, 1);

HalUARTWrite ( HAL_UART_PORT_0, I2Cdata, 3 );
HalI2CReceive(0x52, I2Cdata, 1);

HalUARTWrite ( HAL_UART_PORT_0, I2Cdata, 3 );

通过串口测试发现一直失败。。

请问我的使用过程是否正确?请有经验的朋友分享一下经验!!!