刚刚测试了doorlock 与doorlockcontroller例程,控制作为终端,,接收端为协调器,终端能成功的控制协调器开关,命令能发送出去!那么问题也来了:之前做SampleApp实验时,,里面发送数据都是调用了AF_DataRequest()函数,但是在这个例程里面没找到?请问下大家,doorlockcontroller例程里面数据是通过什么函数发送出去的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
刚刚测试了doorlock 与doorlockcontroller例程,控制作为终端,,接收端为协调器,终端能成功的控制协调器开关,命令能发送出去!那么问题也来了:之前做SampleApp实验时,,里面发送数据都是调用了AF_DataRequest()函数,但是在这个例程里面没找到?请问下大家,doorlockcontroller例程里面数据是通过什么函数发送出去的呢?
我想发送长一点的数据,不是一个命令,而且,这个发送函数,触发的是接收方的哪个事件啊?
触发的是接收方ZCL_INCOMING_MSG。事件处理函数里面对各种命令进行解析处理。
可是AF_DataRequest()函数里面的参数改怎么设置呢?前两个参数以及SAMPLEAPP_TransID这些在DoorLockComtrol的例程里面都没有啊?有HA的例程里有用AF_DataRequest()的示例吗?
HA 引出了ZCL,您可以在zcl.c中看到。举例一下:
ZStatus_t zcl_SendCommand( uint8 srcEP, afAddrType_t *destAddr,
uint16 clusterID, uint8 cmd, uint8 specific, uint8 direction,
uint8 disableDefaultRsp, uint16 manuCode, uint8 seqNum,
uint16 cmdFormatLen, uint8 *cmdFormat )
{
endPointDesc_t *epDesc;
zclFrameHdr_t hdr;
uint8 *msgBuf;
uint16 msgLen;
uint8 *pBuf;
uint8 options;
ZStatus_t status;
epDesc = afFindEndPointDesc( srcEP );
if ( epDesc == NULL )
{
return ( ZInvalidParameter ); // EMBEDDED RETURN
}
#if defined ( INTER_PAN )
if ( StubAPS_InterPan( destAddr->panId, destAddr->endPoint ) )
{
options = AF_TX_OPTIONS_NONE;
}
else
#endif
{
options = zclGetClusterOption( srcEP, clusterID );
// The cluster might not have been defined to use security but if this message
// is in response to another message that was using APS security this message
// will be sent with APS security
if ( !( options & AF_EN_SECURITY ) )
{
afIncomingMSGPacket_t *origPkt = zcl_getRawAFMsg();
if ( ( origPkt != NULL ) && ( origPkt->SecurityUse == TRUE ) )
{
options |= AF_EN_SECURITY;
}
}
}
zcl_memset( &hdr, 0, sizeof( zclFrameHdr_t ) );
// Not Profile wide command (like READ, WRITE)
if ( specific )
{
hdr.fc.type = ZCL_FRAME_TYPE_SPECIFIC_CMD;
}
else
{
hdr.fc.type = ZCL_FRAME_TYPE_PROFILE_CMD;
}
if ( ( epDesc->simpleDesc == NULL ) ||
( zcl_DeviceOperational( srcEP, clusterID, hdr.fc.type,
cmd, epDesc->simpleDesc->AppProfId ) == FALSE ) )
{
return ( ZFailure ); // EMBEDDED RETURN
}
// Fill in the Maufacturer Code
if ( manuCode != 0 )
{
hdr.fc.manuSpecific = 1;
hdr.manuCode = manuCode;
}
// Set the Command Direction
if ( direction )
{
hdr.fc.direction = ZCL_FRAME_SERVER_CLIENT_DIR;
}
else
{
hdr.fc.direction = ZCL_FRAME_CLIENT_SERVER_DIR;
}
// Set the Disable Default Response field
if ( disableDefaultRsp )
{
hdr.fc.disableDefaultRsp = 1;
}
else
{
hdr.fc.disableDefaultRsp = 0;
}
// Fill in the Transaction Sequence Number
hdr.transSeqNum = seqNum;
// Fill in the command
hdr.commandID = cmd;
// calculate the needed buffer size
msgLen = zclCalcHdrSize( &hdr );
msgLen += cmdFormatLen;
// Allocate the buffer needed
msgBuf = zcl_mem_alloc( msgLen );
if ( msgBuf != NULL )
{
// Fill in the ZCL Header
pBuf = zclBuildHdr( &hdr, msgBuf );
// Fill in the command frame
zcl_memcpy( pBuf, cmdFormat, cmdFormatLen );
status = AF_DataRequest( destAddr, epDesc, clusterID, msgLen, msgBuf,
&zcl_TransID, options, AF_DEFAULT_RADIUS );
zcl_mem_free ( msgBuf );
}
else
{
status = ZMemError;
}
return ( status );
}