Other Parts Discussed in Thread: CC2592, Z-STACK, CC2538, CC2591, CC2590
请问:
Z-Stack Home 1.2.2a.44539 协议栈自动控制 CC2538+ CC2592吗? 想找一个 PA 模块,基本都是CCCC2538+CC2592.
但是协议中代码只支持 CC2590, CC2591, 但是模块卖家说支持 CC2592 很困惑?
/* ------------------------------------------------------------------------------------------------
* CC2590/CC2591 support
*
* Define HAL_PA_LNA_CC2590 if CC2538+CC2590EM is used
* Define HAL_PA_LNA if CC2538+CC2591EM is used
* Note that only one of them can be defined
* ------------------------------------------------------------------------------------------------
*/
#define xHAL_PA_LNA
#define xHAL_PA_LNA_CC2590
/* HGM Port and Pin */
#define HGM_BASE GPIO_D_BASE
#define HGM_PIN GPIO_PIN_2
谢谢