This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zstack协议栈之---组网距离-发射功率,接收灵敏度设置 组网距离的问题

Other Parts Discussed in Thread: Z-STACK, CC2530

z-stack 2.4之后,修改发射功率的方法和老版本已经不一样了。

修改发射功率的方法如下:

打开mac_radio_defs.h,找到文件最后面的这段代码:

 


//#define HAL_MAC_USE_REGISTER_POWER_VALUES

//#define HAL_MAC_USE_REGISTER_POWER_VALUES的注释去掉。

变为:

#define HAL_MAC_USE_REGISTER_POWER_VALUES

然后打开ZMain.c

ZMacInit();后面添加如下代码:

{
uint8 value = 0xF5;
MAC_MlmeSetReq(MAC_PHY_TRANSMIT_POWER, &value);
}

  • value与功率的对应关系可以在CC2530的datasheet中找到。


    问:我在测试Z-stack时发现,如果不加NV_RESTORE这个编译选项的话,那么节点必须靠得比较近才能组网成功。
    如果离得较远,就无法组网。请问这是为什么呢?
    答:有两项原因限制了zigbee节点的加入网络的距离,一个是默认发射功率为0dbm,另一个是节点加入是要求信号强度-84dbm以上,修改这两个条件可以使用zigbee节点可以在较远的地方加入网络。如果打开NV_Restore并且成功加入过网络,节点可以在小于-84dbm信号强度下通讯,这就是为什么打开nv_restore,可以有较远的距离的原因。
    问:如何修改-84dbm这个值?
    答:修改mac_spec.h中的MAC_SPEC_ED_MIN_DBM_ABOVE_RECEIVER_SENSITIVITY,将其改为1

    #define MAC_SPEC_ED_MIN_DBM_ABOVE_RECEIVER_SENSITIVITY 10
    另外还要把MAC_SPEC_MIN_RECEIVER_SENSITIVITY,改成-94

    #define MAC_SPEC_MIN_RECEIVER_SENSITIVITY -85

  • 你这个修改功率的方法,还是第一次听说,对有RF前端的方案无效。