This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想问下在只使用CC2650/CC2630芯片时,能否使用ZigBee HA 协议进行网状网络的组网?我看了你们的例子“C:\ti\simplelink\zstack_home_1_02_02a_44539\Projects\zstack\HomeAutomation”,按我自己的理解,例子中“ZStackCore-EndDevice”应该是将工程编译成终端设备,而“SampleSwitch-SmartRF06” 应该是作为终端设备使用时项目的各种应用层部分。
如果我要用CC2650/CC2630进行组网,我要怎么做?使用哪个CC2650/2630的工程进行开发与测试?
参考Z-Stack Home Sample Application User's Guide可知
Seven sample applications are included in the Z-Stack Home installer: SampleDoorLock,SampleDoorLockController, SampleLight, SampleSwitch, SampleHeatingCoolingUnit, SampleTemperatureSensor, SampleThermostat, and the SensorTag sample application supported
only on the CC2650 SensorTag. Each of them supports Coordinator, Router and End Device configurations when used with CC253x platforms and in CC2630/CC2650 platforms End Device is the only configuration supported.