// This is an index into table Requested Timeout Enumerated Values.
// It is used by the parent router, it indicates the default timeout value
// for any end device that does not negotiate a different timeout value
uint8 zgNwkEndDeviceTimeoutDefault = NWK_END_DEV_TIMEOUT_DEFAULT;
//========== Child Aging END DEVICE configuration ===============
// Values used by End Device when sending End Device Timeout Request
uint8 zgEndDeviceTimeoutValue = END_DEV_TIMEOUT_VALUE;
uint8 zgEndDeviceConfiguration = END_DEV_CONFIGURATION;
请问zgNwkEndDeviceTimeoutDefault 所指的时间枚举表是哪个,这个变量的含义是什么,如果EndDevice没有开启childaging,而在路由开启了,路由会把zgNwkEndDeviceTimeoutDefault 时间认为是没有收到data request的超时时间吗
//timeoutValue[15]
// 10, // 0 10 seconds
// 2, // 1 2 minutes
// 4, // 2 4 minutes
// 8, // 3 8 minutes
// 16, // 4 16 minutes
// 32, // 5 32 minutes
// 64, // 6 64 minutes
// 128, // 7 128 minutes
// 256, // 8 256 minutes
// 512, // 9 512 minutes
// 1024, // 10 1024 minutes
// 2048, // 11 2048 minutes
// 4096, // 12 4096 minutes
// 8192, // 13 8192 minutes
// 16384 // 14 16384 minutes
//
是指这个表吗