设备为cc2530+cc2592,协议栈中对应的PA宏定义和引脚我都改动了,但是通过万用表上发现设备最大电流就30-40ma左右与官方手册中有出入。
设置发射功率的函数:
macRadioSetTxPower(0xF5);
macRadioUpdateTxPower();
ZMacSetTransmitPower(TX_PWR_PLUS_19);
测试方式:入网后,就开启一个5ms的发送数据任务,接着通过万用表看电流
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.