This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

smartRF studio测试packet TX和RX时接收端NOK包突增512的原因

Other Parts Discussed in Thread: CC2591, CC2530, CC2531

环境:win7 32位操作系统、WIFI环境下、空旷地点

软件smart_studio7

设备:CC2530+CC2591(主机)与CC2530(节点)

实验:测试两者收发包通信时的丢包率

设置:expert mode模式,主机range exteender设置为CC2591,tx power设置成20db,节点range extender设置为none,tx设置为4.5db,收发包数量是2000包

发送端没有勾选Add Seq.Number,接受端有勾选

出现的问题:

1、不管是主机发送节点接受还是反过来在收发包测试时接受端经常会突然收到512包NOT OK包,如果多接收几次就会因为超过2000包而停止,多数这个时候接收OK的包与发送端发出的包数量相当,且未达到设置的2000包。

2、同上在测试时NOT OK包突增,但会随着OK包的增多而慢慢增减。

请教下出现以上两个问题的原因是?