Other Parts Discussed in Thread: CC2652R, CC2538, CC2530, CC2650, Z-STACK
用CC2652组网,ZigBee3.0协议,最多可以支持多少个节点,CC2652可以做路由的吧?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我只能给你一些建议,如果你用CC2652R去做,需要考虑的是
• NWK_MAX_DEVICE_LIST
• MAX_NEIGHBOR_ENTRIES
• MAX_RTG_SRC_ENTRIES
• ZDSECMGR_TC_DEVICE_MAX
您好,z-stack3.0协议栈中ZDSecMgr.h文件中有如下代码段
是使用的3.0协议栈,参考的MTO方案,节点加到39个的时候就加不上去了,入网失败的原因不是因为网络风暴什么的,而是节点入网的时候发送request key,ZC不再答复transport key 报文,节点问三次后ZC就发送remove指令了,所以我怀疑有因素限制入网个数了,这查了一周可能的地方才找到这个ZDSECMGR_TC_DEVICE_MAX宏,然后看了你上面给人家回复的贴子,4个选项除了这个我没动过之外我设置的应该都没问题,而且这个限制也比较符合我的实验结果,所以才问的,我肯定还要做实验,但是我没必要搭建一个好几十的节点才验证这里的限制吧,问你的意思就是想在实验前最大化知道这两个宏的作用,我完全可以将这两个值改小,如果能复现我之前的问题,基本就能确定是这个地方限制了网络中节点个数。