Other Parts Discussed in Thread: CC2530
cc2530 z3.0
我怎么一开启MT-TASK 和 ZTOOL_P1就报错
Error[e16]: Segment XDATA_I (size: 0x140 align: 0) is too long for segment definition. At least 0x114 more bytes needed.
The problem occurred while processing the segment placement command
"-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available
memory ranges were "XDATA:1ed4-1eff"
Reserved ranges relevant to this placement:
XDATA:1-300 XSTACK
XDATA:301-1eff XDATA_Z
BIT:0-7 BREG
BIT:80-87 SFR_AN
BIT:90-97 SFR_AN
BIT:a8-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:f8-ff SFR_AN
Error while running Linker
不开启的时候是正常的