Other Parts Discussed in Thread: Z-STACK
如提。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我先试着把空中来的数据,改成64bit输出到串口看看,从下面这个ZDApp.c来看,是ZDP_IncomingData函数收到了数据,
void ZDApp_ProcessOSALMsg( osal_event_hdr_t *msgPtr )
{
// Data Confirmation message fields
uint8 sentEP; // This should always be 0
uint8 sentStatus;
afDataConfirm_t *afDataConfirm;
uint8 tmp;
switch ( msgPtr->event )
{
// Incoming ZDO Message
case AF_INCOMING_MSG_CMD:
ZDP_IncomingData( (afIncomingMSGPacket_t *)msgPtr );
break;
case ZDO_CB_MSG:
ZDApp_ProcessMsgCBs( (zdoIncomingMsg_t *)msgPtr );
break;
case AF_DATA_CONFIRM_CMD:
// This message is received as a confirmation of a data packet sent.
// The status is of ZStatus_t type [defined in NLMEDE.h]
// The message fields are defined in AF.h
afDataConfirm = (afDataConfirm_t *)msgPtr;
sentEP = afDataConfirm->endpoint;
sentStatus = afDataConfirm->hdr.status;
...
}
然后再跳到这个函数,就不知道改哪儿了
void ZDP_IncomingData( afIncomingMSGPacket_t *pData )
{
uint8 x = 0;
uint8 handled;
zdoIncomingMsg_t inMsg;
inMsg.srcAddr.addrMode = Addr16Bit;
inMsg.srcAddr.addr.shortAddr = pData->srcAddr.addr.shortAddr;
osal_memcpy(inMsg.srcAddr.addr.extAddr, pData->srcAddr.addr.extAddr, 8); //zjt
inMsg.wasBroadcast = pData->wasBroadcast;
inMsg.clusterID = pData->clusterId;
inMsg.SecurityUse = pData->SecurityUse;
inMsg.asduLen = pData->cmd.DataLength-1;
inMsg.asdu = pData->cmd.Data+1;
inMsg.TransSeq = pData->cmd.Data[0];
inMsg.macDestAddr = pData->macDestAddr;
handled = ZDO_SendMsgCBs( &inMsg );
#if (defined MT_ZDO_CB_FUNC)
#if !defined MT_TASK
if (zgZdoDirectCB)
#endif
{
MT_ZdoDirectCB( pData, &inMsg );
}
#endif
while ( zdpMsgProcs[x].clusterID != 0xFFFF )
{
if ( zdpMsgProcs[x].clusterID == inMsg.clusterID )
{
zdpMsgProcs[x].pFn( &inMsg );
return;
}
x++;
}
// Handle unhandled messages
if ( !handled )
ZDApp_InMsgCB( &inMsg );
}