This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2630组网及组网终端数量

Other Parts Discussed in Thread: CC2538, CC2630, CC2530, CC2652R

我想使用Zigbee组网,将终端采集的数据及状态发送到PC机上,组网终端数量需满足至少100个。

打算使用CC2630芯片,搜到的资料是CC2630不能单独用作路由和协调器,是否可以用CC2538左右路由和协调器,终端采用CC2630的方案,终端数量能否满足要求?

如果不行,直接采用CC2530用作终端、路由、协调器,估计可支持的最大终端是多少?

另外,我的终端是会分布在不同的房间(一个房间可能有2-3个),是否需要加增益芯片?

谢谢