This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zigbee ota升级



End Device – OTAClient - ImageA - withBootloader 这个工程ota版本默认为00000001,类型默认为2538  ;请问这些默认值可以修改吗??

  • #if defined __IOCC2538_H__
    const preamble_t OTA_Preamble @ ".preamble" =
    {
    HAL_OTA_RC_MAX, // Default program length of max if not using post-processing tool.
    OTA_MANUFACTURER_ID, // Manufacturer ID
    OTA_TYPE_ID, // Image Type
    0x00000001 // Image Version
    };
    版本可以改其他不能修改,你在升级时候会校验你的升级固件版本,升级的版本必须要比现在运行的版本高才可以(PS:除非你把校验的程序屏蔽掉)