This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

协调器如何在应用层处理路由器发送来的“update device command”命令?

Other Parts Discussed in Thread: Z-STACK, CC2538

协议栈:Z-Stack 3.0.1

处理器:CC2538

情况描述:网络中有一个协调器,一个路由器和一个终端节点,终端节点的父节点为路由器。当终端节点利用按键“恢复出厂设置”时,会广播范围为1的“Leave”命令。此时身为父节点的路由器收到“Leave”命令会发送一条“update device command”给协调器,我想在协调器的应用层利用这一条信息做终端节点的出网通知,可是找不到“update device command”命令的回调函数。找到的“ZDO_UpdateDeviceIndication()”也不能使用。

提出的问题:请问可以在协调器的应用层上处理“update device command”命令吗,如何处理?除了用这个方法实现子设备出网通知以外还有什么方法吗?

谢谢!