This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Z-STACK3.0.1编绎出错

Other Parts Discussed in Thread: CC2530, CC2652R, CC2538

麻烦各位大神帮解决一下:

Z-STACK3.0.1

IAR FOR 8051 10.20.1

使用Z-STACK3.0.1中的原始例程“SampleSwitch”。编绎协调器设备时,开启了ZTOOL_P1、MT_TASK后报错如下:

Error[e16]: Segment XDATA_I (size: 0x122 align: 0) is too long for segment definition. At least 0x93 more bytes needed. The problem occurred while processing the segment
placement command "-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available memory ranges were
"XDATA:1e71-1eff"
Reserved ranges relevant to this placement:
XDATA:1-300 XSTACK
XDATA:301-1eff XDATA_Z
BIT:0-7 BREG
BIT:80-87 SFR_AN
BIT:90-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:e8-ef SFR_AN
BIT:f8-ff SFR_AN
Error while running Linker

路由器没有问题

求解!!!