This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2530低功耗硬件方面的问题

Other Parts Discussed in Thread: CC2530

咨询一点问题:

我想要做一些低功耗的设备,关于硬件方面有没有什么需要注意的地方?功耗尽量降到最低

  • 基本上都是軟體設定,硬體上面應該還好
  • 如果我想不使用32.768KHZ的外部晶振,请问一下,软件改怎么设置?我使用的是PM2 休眠模式,不使用外部晶振,会不会造成什么影响?
  • 请教一下,我想要在ZStack 1.2.2a中不使用外部32KHZ的晶振,程序中需要怎么设置?关闭外部晶振会造成什么影响吗?

  • 可以參考CC2530 user guide的說明

    4.4.3 32-kHz Oscillators
    Two 32-kHz oscillators are present in the device as clock sources for the 32-kHz clock:
    • 32-kHz XOSC
    • 32-kHz RCOSC
    By default, after a reset, the 32-kHz RCOSC is enabled and selected as the 32-kHz clock source. The
    RCOSC consumes less power, but is less accurate compared to the 32-kHz XOSC. The chosen 32-kHz
    clock source drives the Sleep Timer, generates the tick for the Watchdog Timer, and is used as a strobe in
    Timer 2 to calculate the Sleep Timer sleep time. The CLKCONCMD.OSC32K register bit selects the
    oscillator to be used as the 32-kHz clock source. This bit does not give an indication of the stability of the
    32-kHz XOSC.
    The CLKCONCMD.OSC32K register bit can be written at any time, but does not take effect before the 16-
    MHz RCOSC is the active system clock source. When system clock is changed from the 16-MHz RCOSC
    to the 32-MHz XOSC (CLKCONCMD.OSC from 1 to 0), calibration of the 32-kHz RCOSC starts up and is
    performed once if the 32-kHz RCOSC is selected. During calibration, a divided version of the 32-MHz
    XOSC is used. The result of the calibration is that the 32-kHz RSOSC is running at 32.753 kHz. The 32-
    kHz RCOSC calibration may take up to 2 ms to complete. Calibration can be disabled by setting
    SLEEPCMD.OSC32K_CALDIS to 1. At the end of the calibration, an extra pulse may occur on the 32-kHz
    clock source, which causes the sleep timer to be incremented by 1.
    Note that after having switched to the 32-kHz XOSC and when coming up from PM3 with the 32-kHz
    XOSC enabled, the oscillator requires up to 500 ms to stabilize on the correct frequency. The Sleep
    Timer, Watchdog Timer and clock-loss detector should not be used before the 32-kHz XOSC is stable.
  • 可以參考CC2530 user guide的說明

    4.4.3 32-kHz Oscillators
    Two 32-kHz oscillators are present in the device as clock sources for the 32-kHz clock:
    • 32-kHz XOSC
    • 32-kHz RCOSC
    By default, after a reset, the 32-kHz RCOSC is enabled and selected as the 32-kHz clock source. The
    RCOSC consumes less power, but is less accurate compared to the 32-kHz XOSC. The chosen 32-kHz
    clock source drives the Sleep Timer, generates the tick for the Watchdog Timer, and is used as a strobe in
    Timer 2 to calculate the Sleep Timer sleep time. The CLKCONCMD.OSC32K register bit selects the
    oscillator to be used as the 32-kHz clock source. This bit does not give an indication of the stability of the
    32-kHz XOSC.
    The CLKCONCMD.OSC32K register bit can be written at any time, but does not take effect before the 16-
    MHz RCOSC is the active system clock source. When system clock is changed from the 16-MHz RCOSC
    to the 32-MHz XOSC (CLKCONCMD.OSC from 1 to 0), calibration of the 32-kHz RCOSC starts up and is
    performed once if the 32-kHz RCOSC is selected. During calibration, a divided version of the 32-MHz
    XOSC is used. The result of the calibration is that the 32-kHz RSOSC is running at 32.753 kHz. The 32-
    kHz RCOSC calibration may take up to 2 ms to complete. Calibration can be disabled by setting
    SLEEPCMD.OSC32K_CALDIS to 1. At the end of the calibration, an extra pulse may occur on the 32-kHz
    clock source, which causes the sleep timer to be incremented by 1.
    Note that after having switched to the 32-kHz XOSC and when coming up from PM3 with the 32-kHz
    XOSC enabled, the oscillator requires up to 500 ms to stabilize on the correct frequency. The Sleep
    Timer, Watchdog Timer and clock-loss detector should not be used before the 32-kHz XOSC is stable.
  • 硬件上要考虑好功耗控制问题,这牵涉到你具体要实现什么功能,用什么电路实现,比较CC2530只是控制和无线传输,其他需要外部电路实现的部分要完全受控,另外有模电的部分也要考虑好功耗问题。
  • CC2530已经选定了,硬件参数已经定了,所以硬件没啥可注意的。
    在软件上,降低发送次数,空闲时进入休眠状态;关闭不必要的外设时钟等。
  • 用内部晶振的话,精确度方面稍有不足。你看一下应用对这块是否有要求,大部分是推荐用外部的
  • 在硬件基本上差不多的条件下,要想解决低功耗的问题,可以从以下两个方面着手:
    1.软件算法
    2.电路拓扑
  • 软件上设置低功耗的睡眠模式,关掉不适用的I/O口,降低时钟频率等

  • 硬件方面应该就是配置该芯片的电路,能精减则精减,软件上需要注意IO收发频率,数据计算等等,还是建议用外部晶振,比较可靠些