This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZIGBEE芯片在组网应用中如何实现信息传输的

在上百个节点组网中,每个节点给中继发送信息;是如何实现通道空闲检测的,具体原理是什么。

  • 基本上就是打開RX看看目前通道有沒有信號,沒有的話代表通道空闲

  • According to the IEEE 802.15.4 protocol, the unslotted CSMA/CA algorithm is similar to the slotted CSMA/CA algorithm, besides that it is used in the non-Beacon-enabled mode. In the unslotted CSMA/CA, each time a device wishes to transmit data frames or MAC commands, it waits for a random period. If the channel is found to be idle (done by CCA mechanism), following the random back-off, the device transmits its data. If the channel is found to be busy following the random back-off, the device waits for another random period before trying to access the channel again. Acknowledgment frames are sent without using a CSMA-CA mechanism.