This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

能不能关闭Zstack 2.5.1中的重传机制呢?

请问下能不能关闭Zstack 2.5.1中的重传机制呢?在f8wconfig配置文件也已经将DAPSC_MAX_FRAME_RETRIES置0了,而且把maxFrameRetries也置0了,还有把mac_api.h中的MAC_TXOPTION_ACK 的0x01也改为了0x00,试图关闭mac ACK 。我看了几乎所有论坛上关于这个发包1000个,收到超过1000个包的问题,而且提问者也都是把这些参数修改后,还是会出现重传的问题。但是最后TI员工后面并没有说清楚啊。

  总结就是:Zstack中的重传机制可以关闭吗?如何关闭呢?究其根本还是对这个重传机制没有彻底弄明白。

  可不可以正面回答下这个问题呢?困惑了很久,非常感谢TI大佬们。