Other Parts Discussed in Thread: CC2530, CC2538, CC2531, CC2652R
Error[e16]: Segment XDATA_I (size: 0xd5 align: 0) is too long for segment definition. At least 0x38 more bytes needed. The problem
occurred while processing the segment placement command "-Z(XDATA)XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END",
where at the moment of placement the available memory ranges were "XDATA:1e63-1eff"
Reserved ranges relevant to this placement:
XDATA:1-300 XSTACK
XDATA:301-1eff XDATA_Z
BIT:0-7 BREG
BIT:80-97 SFR_AN
BIT:a0-af SFR_AN
BIT:b8-c7 SFR_AN
BIT:d8-df SFR_AN
BIT:e8-ef SFR_AN
BIT:f8-ff SFR_AN
Error while running Linker
请问这个错误该怎么解决?我定义了一个白名单数组,当数组元素个数小于70没有问题,大于70就会报错。