This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

问一个ZIGBEE组网的基础问题

请问一个coordinator在组网的时候是不是只使用了一个5M带宽的频点,如果在一个局域网内想组大网,是不是可以让另一个coordinator用另一个5M频点?谢谢。

  • * Default channel is Channel 11 - 0x0B */
    // Channels are defined in the following:
    // 0 : 868 MHz 0x00000001
    // 1 - 10 : 915 MHz 0x000007FE
    // 11 - 26 : 2.4 GHz 0x07FFF800
    //
    //-DMAX_CHANNELS_868MHZ 0x00000001
    //-DMAX_CHANNELS_915MHZ 0x000007FE
    //-DMAX_CHANNELS_24GHZ 0x07FFF800
    //-DDEFAULT_CHANLIST=0x04000000 // 26 - 0x1A
    //-DDEFAULT_CHANLIST=0x02000000 // 25 - 0x19
    //-DDEFAULT_CHANLIST=0x01000000 // 24 - 0x18
    //-DDEFAULT_CHANLIST=0x00800000 // 23 - 0x17
    //-DDEFAULT_CHANLIST=0x00400000 // 22 - 0x16
    //-DDEFAULT_CHANLIST=0x00200000 // 21 - 0x15
    //-DDEFAULT_CHANLIST=0x00100000 // 20 - 0x14
    //-DDEFAULT_CHANLIST=0x00080000 // 19 - 0x13
    //-DDEFAULT_CHANLIST=0x00040000 // 18 - 0x12
    //-DDEFAULT_CHANLIST=0x00020000 // 17 - 0x11
    //-DDEFAULT_CHANLIST=0x00010000 // 16 - 0x10
    //-DDEFAULT_CHANLIST=0x00008000 // 15 - 0x0F
    //-DDEFAULT_CHANLIST=0x00004000 // 14 - 0x0E
    //-DDEFAULT_CHANLIST=0x00002000 // 13 - 0x0D
    //-DDEFAULT_CHANLIST=0x00001000 // 12 - 0x0C
    -DDEFAULT_CHANLIST=0x00000800 // 11 - 0x0B

    通常是一个ZC,然后通过加路由的方式,做一个MTO网络。
  • 可以的,但是如果你的大网沒有很大其實沒有必要,我曾經在辦公桌上設置過660個設備在同一個大网都沒有問題

  • 多谢。这个解决方案是为某些极端情况下准备的。总觉的2.4这么多频点不用白不用啊。
  • 频点很多但是有些跟WiFi/ble會重疊,所以在組網的時候會建議避開