This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530用路由器建立分布式网络

用户手册中关于分布式网络的介绍我就找到了10.4这一段,有没有更详细的介绍,关于分布式网络的地址分配、数据传输等其他的详细内容???

10.4 Distributed security network
This network type can be formed by network-forming router devices. In this network topology, all the nodes have
the ability to open the network for joining and any router device can deliver the network key to a joining device. The
network key will be encrypted at APS layer with a Default Distributed Global key, in section 10.5.3. This network
key will be delivered via an APS Transport Key Command in which the TC address will be set to
0xFFFFFFFFFFFFFFFF, which tells the joining device it is joining a distributed security network. The application
can consult the value of AIB_apsTrustCenterAddress to see if it has joined a distributed network.
It is important to note that after a distributed network is formed, the network key cannot be updated because there is
no defined method of securely distributing a network key in a network with this topology.