This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530芯片的IO引脚P2.3和P2.4我们可以使用吗

Other Parts Discussed in Thread: CC2530

问题一:在数据手册上看见CC2530有21个引脚可用,但是为什么我的原理图上没有看见P2.3和P2.4这两个引脚,现在不知道这两个引脚用来做什么了。因为现在我在开发的一个项目,进入PM2状态以后电流还是保持在3mA左右,检查其他io口状态的时候发现的没有配置这两个引脚,我是否可以吧这两个io口置成上拉输入的状态。

问题二:还是上面一个项目,平时UART0的引脚作为端口使用,来检测是否有数据到来,进入低功耗,如果有数据我就将这两个端口转化为串口模式传输数据,这样在PM2状态下功耗会有什么影响吗,因为这个功耗的问题一直解决不了。

在低功耗的状态下我看睡眠的时间发现应该是正常的,但是电流就是降不下去!希望有解答,谢谢!!