This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我想使用简单的加密。设置如下:
-DSECURE=1
zgPreConfigKeys=TRUE
每个设备中均定义相同的default;
总共四个设备,一个协调器+终端1+终端2 是开启加密的。还有一个终端3是普通节点未加密的。
协调器上电,终端1上电,入网成功,网络地址为31087。
终端3上电,好像也入网成功了,并且分配了地址,但是不能相互通信。
终端2上电,入网成功,网络弟子为31089。
问题:终端3占用了一个网络地址,每个协调器中可连入的设备是由有限的,如果有很多终端3这样的设备,会不会导致终端1、2无法入网。