This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC110L经常会有非预期的脉冲,读RXBYTES(3B),有时是0,有时是一个比较大的数。

Other Parts Discussed in Thread: CC110L

CC110L的GPIO0设置为06时,经常会有非预期的脉冲,这个时候读CC110L RXBYTES(3B),要不是0,要不是比较大的数,出现大数后,如果不重新初始化TI110L,就再也收不到数据了,重新初始化可以继续接受数据;但是那个非预期脉冲根据不同的参数出现不同的状况。请帮解释出现这现象的原因,怎样避免。

  • 你说的是GDO 0吧?
    Setting PKTCTRL0.PKT_FORMAT to 1 enables synchronous serial mode. When using this mode, sync
    detection should be disabled together with CRC calculation ( MDMCFG2.SYNC_MODE=000 and
    PKTCTRL0.CRC_EN=0). Infinite packet length mode should be used (
    PKTCTRL0.LENGTH_CONFIG=10b).
    In synchronous serial mode, data is transferred on a two-wire serial interface. The CC110L provides a
    clock that is used to set up new data on the data input line or sample data on the data output line. Data
    input (TX data) is on the GDO0 pin. This pin will automatically be configured as an input when TX is
    active. The TX latency is 8 bits. The data output pin can be any of the GDO pins. This is set by the
    IOCFG0.GDO0_CFG, IOCFG1.GDO1_CFG, and IOCFG2.GDO2_CFG fields. The RX latency is 9 bits.
    The MCU must handle preamble and sync word detection in software.
    The MCU must handle preamble and sync word insertion/detection in software, together with CRC
    calculation and insertion.

    你设置为06 代表
    Asserts when sync word has been sent / received, and de-asserts at the end of the packet. In RX, the pin will also de-assert
    when a packet is discarded due to address or maximum length filtering or when the radio enters RXFIFO_OVERFLOW state.
    In TX the pin will de-assert if the TX FIFO underflows.

    建议参考下面的帖子修改:
    e2e.ti.com/.../139985