Other Parts Discussed in Thread: CC2530
未使用cc2530 的Uart1的位置一作为SPI,配置如下,请问配置是否正确,SPI速率设置 具体怎么设置 我要实现3MHZ以下的速率 应该怎么设置
PERCFG &= ~0x02; // PERCFG.U1CFG = 0
P0SEL |= 0x38; // P0_5, P0_4, and P0_3 are peripherals
P0SEL &= ~0x04; // P0_2 is GPIO (SSN)
P0DIR |= 0x04; // SSN is set as output
U1BAUD = 216;
U1GCR &= 0xE0;
U1GCR |= 0x11; // BAUD_E = 17
U1GCR |= 0x20;//MSB_FIRST