This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530可以使用868MHZ的频率吗?



/* Default channel is Channel 11 - 0x0B */
// Channels are defined in the following:
//         0      : 868 MHz     0x00000001
//         1 - 10 : 915 MHz     0x000007FE
//        11 - 26 : 2.4 GHz     0x07FFF800
//
//-DMAX_CHANNELS_868MHZ     0x00000001
//-DMAX_CHANNELS_915MHZ     0x000007FE
//-DMAX_CHANNELS_24GHZ      0x07FFF800