您好!
我在用DIO8作模拟SCLK时,频率要求1MH。如何将它设置为high speed 模式呢?
SClK | PIN_GPIO_OUTPUT_EN | PIN_GPIO_LOW | PIN_PUSHPULL | PIN_DRVSTR_MAX,
外部的晶振我们用的24MHz, IO由0到1,测得的频率就为1.5us,也就是说频率的极值为:330KHz,如何设置IO的高频模式呢?
是通过设对 CLK32KCTL Register 来实现吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.