This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

终端节点设备唤醒后上报数据报错0x10

Other Parts Discussed in Thread: CC2530

平台是cc2530 +z-stack3.0.1,使用enddevice类型设备。

在设备初次上电并找网完成之后,通过zcl_SendReportCmd函数上报数据正常。但是当低功耗设备进入睡眠之后通过外部中断唤醒,当使用相同的函数上报相同的数据时,每次都返回错误0x10.

zcl_SendReportCmd返回0x10错误是什么原因?为什么在未睡眠之前可以发送成功,睡眠唤醒之后就一直返回0x10?

  • 0x10是指ZMemError,申请内存失败。你的网络里有几个节点?
  • 你使用zcl_SendReportCmd的相關程序貼上來看一下
  • uint8 DataBuff[16] = {0};

    zclReportCmd_t* reportCmd = osal_mem_alloc( sizeof( zclReportCmd_t ) + sizeof( zclReport_t ));
    if(reportCmd != NULL)
    {
    reportCmd->numAttr = 1;
    reportCmd->attrList[0].attrID = ATTRID_BASIC_SMART_LOCK_DATA;
    reportCmd->attrList[0].dataType = ZCL_DATATYPE_CHAR_STR;
    DataBuff[0] = len;
    memcpy(DataBuff + 1,buff,len);
    memcpy(SmartLockData,DataBuff,len + 1);
    reportCmd->attrList[0].attrData = SmartLockData;

    if(ZDApp_GetState() == DEV_END_DEVICE && zoneState == SS_IAS_ZONE_STATE_ENROLLED)
    {
    HalLedSet(led_red, HAL_LED_MODE_ON);
    osal_start_timerEx(ias_TaskID, SAMPLEAPP_TURN_OFF_RED, 100);//亮灯
    ZStatus_t status = zcl_SendReportCmd(SAMPLESW_ENDPOINT, &zclSampleSw_DstAddr, ZCL_CLUSTER_ID_GEN_BASIC,
    reportCmd, ZCL_FRAME_SERVER_CLIENT_DIR, TRUE, zclSampleSwSeqNum++);

    }

    这是使用zcl_SendReportCmd函数的相关代码,就是此处status返回0x10错误。

    ZStatus_t zcl_SendReportCmd( uint8 srcEP, afAddrType_t *dstAddr,
    uint16 clusterID, zclReportCmd_t *reportCmd,
    uint8 direction, uint8 disableDefaultRsp, uint8 seqNum )
    {
    uint16 dataLen = 0;
    uint8 *buf;
    ZStatus_t status;
    uint8 i;

    // calculate the size of the command
    for ( i = 0; i < reportCmd->numAttr; i++ )
    {
    zclReport_t *reportRec = &(reportCmd->attrList[i]);

    dataLen += 2 + 1; // Attribute ID + data type

    // Attribute Data
    dataLen += zclGetAttrDataLength( reportRec->dataType, reportRec->attrData );
    }

    buf = zcl_mem_alloc( dataLen );
    if ( buf != NULL )
    {
    // Load the buffer - serially
    uint8 *pBuf = buf;

    for ( i = 0; i < reportCmd->numAttr; i++ )
    {
    zclReport_t *reportRec = &(reportCmd->attrList[i]);

    *pBuf++ = LO_UINT16( reportRec->attrID );
    *pBuf++ = HI_UINT16( reportRec->attrID );
    *pBuf++ = reportRec->dataType;

    pBuf = zclSerializeData( reportRec->dataType, reportRec->attrData, pBuf );
    }

    status = zcl_SendCommand( srcEP, dstAddr, clusterID, ZCL_CMD_REPORT, FALSE,
    direction, disableDefaultRsp, ReportMandCode, seqNum, dataLen, buf );
    zcl_mem_free( buf );
    }
    else
    {
    status = ZMemError;
    }

    return ( status );
    }

    这是zcl_SendReportCmd函数,用的是协议栈自带的版本,没有做改动,其中修改ReportMandCode=0x1249.

  • 网络里只有此低功耗节点和协调器两个设备