基于home stack1.2.2a开发CC2630,CC2630做终端,CC2530做协调器。开启EZMODE后发现CC2630不能入网,下面是抓包信息,不知该如何调试解决?希望可以得到回复,感谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,重新查看了程序,已经执行了zcl_EZModeAction( EZMODE_ACTION_NETWORK_STARTED, NULL );,CC2530和CC2630都开启了EZMODE。之后就一直重复抓包文件里的数据帧,不知是哪里的问题?而且我这个抓包程序是不是也有点跟通常的不太一样,我看其他的抓包都能显示当前包的类型,我这个好像没有。CC2630程序是在TemperatureSensor的基础上改的终端程序,CC2530是在SampleSwitch的基础上改的协调器。抓包2.psd
没有取消,CC2530是通过识别一个UART指令后建立网络。
SECURE=1
TC_LINKKEY_JOIN
NV_INIT
NV_RESTORE
HOLD_AUTO_START
ZTOOL_P1
MT_TASK
xMT_APP_FUNC
MT_SYS_FUNC
xMT_ZDO_FUNC
xLCD_SUPPORTED=DEBUG
MULTICAST_ENABLED=FALSE
ZCL_READ
ZCL_WRITE
ZCL_REPORT
ZCL_EZMODE
ZCL_BASIC
ZCL_IDENTIFY
xZCL_ON_OFF
ZCL_DIAGNOSTIC
FEATURE_SYSTEM_STATS
以上CC2530的配置。
以下是CC2630的配置。
ZCL_READ
ZCL_WRITE
ZCL_BASIC
ZCL_REPORT
ZCL_IDENTIFY
ZCL_PRESSURE_MEASUREMENT
ZCL_EZMODE
xZCL_GROUPS
ZCL_STANDALONE
ZG_SECURE_ENABLED
ewarm
USE_ICALL
HEAPMGR_SIZE=4096
ICALL_HOOK_ABORT_FUNC=halAssertHandler
xdc_runtime_Log_DISABLE_ALL
xdc_runtime_Assert_DISABLE_ALL
MODULE_CC26XX_5X5
xTI_DRIVERS_LCD_INCLUDED
取消hold_auto_start后全部是NWL UNKNOWN COMMAND抓包3.psd