This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 zstack 3.0.2串口问题



串口0初始化如下,即收发线为P0.2和P0.3

void initUart0()
{
  halUARTCfg_t uartConfig;
 
  /* Initialize APP ID */
  App_TaskID = 0;
 
  uartConfig.configured = TRUE;
  uartConfig.baudRate = HAL_UART_BR_4800;//HAL_UART_BR_9600;
  uartConfig.flowControl = FALSE;
  uartConfig.flowControlThreshold = 0;
  uartConfig.rx.maxBufSize = 240;//默认128;
  uartConfig.tx.maxBufSize = 240;//默认128;
  uartConfig.idleTimeout = 6;
  uartConfig.intEnable = TRUE;
  uartConfig.callBackFunc = uartRxCb;
  HalUARTOpen (HAL_UART_PORT_0, &uartConfig);
}

以上初始化已经关闭了流控制,我想把P0.4和P0.5用作GPIO(我在初始化里已经把P0.4和P0.5用作GPIO还是不行),

但是怎么都不行,一直查找发现以下代码,串口例程默认的是DMA,

我关闭的流控制,下面的代码怎么又自动打开了?(我在初始化里已经把P0.4和P0.5用作GPIO还是不行),

static uint16 HalUARTReadDMA(uint8 *buf, uint16 len)

{

……

PxOUT &= ~HAL_UART_Px_RTS;  // Re-enable the flow on any read.

……

}

我只想用P0.2和P0.3收发数据即可,P0.4和P0.5用作普通IO,请问怎么配置?(我在初始化里已经把P0.4和P0.5用作GPIO根本不起作用)