This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求助:如何让CC2538 3.0.2的历程HomeAutomation 里GenericApp 做协调器和CC2530 2.5.a 里的Samples里SampleApp终端通讯?

Other Parts Discussed in Thread: CC2538, CC2530

如何让CC2538 3.0.2的历程HomeAutomation 里GenericApp 做协调器和CC2530 2.5.a 里的Samples 里SampleApp终端通讯?

已经测试让CC2538 建立了网络,密钥安全关闭,网络id  ffff任意  并且描述也改成和cc2530一样

// This list should be filled with Application specific Cluster IDs.
const cId_t SampleApp_ClusterList[SAMPLEAPP_MAX_CLUSTERS] =
{
SAMPLEAPP_PERIODIC_CLUSTERID,
SAMPLEAPP_FLASH_CLUSTERID
};

const SimpleDescriptionFormat_t SampleApp_SimpleDesc =
{
SAMPLEAPP_ENDPOINT, // int Endpoint;
SAMPLEAPP_PROFID, // uint16 AppProfId[2];
SAMPLEAPP_DEVICEID, // uint16 AppDeviceId[2];
SAMPLEAPP_DEVICE_VERSION, // int AppDevVer:4;
SAMPLEAPP_FLAGS, // int AppFlags:4;
SAMPLEAPP_MAX_CLUSTERS, // uint8 AppNumInClusters;
(cId_t *)SampleApp_ClusterList, // uint8 *pAppInClusterList;
SAMPLEAPP_MAX_CLUSTERS, // uint8 AppNumInClusters;
(cId_t *)SampleApp_ClusterList // uint8 *pAppInClusterList;
};

// Fill out the endpoint description.
SampleApp_epDesc.endPoint = SAMPLEAPP_ENDPOINT;
SampleApp_epDesc.task_id = &SampleApp_TaskID;
SampleApp_epDesc.simpleDesc
= (SimpleDescriptionFormat_t *)&SampleApp_SimpleDesc;
SampleApp_epDesc.latencyReq = noLatencyReqs;

// Register the endpoint description with the AF
afRegister( &SampleApp_epDesc );

CC2530 SampleApp历程终端里的描述不变同上,密钥安全关闭,网络id  ffff任意  

CC2530表现一直在寻网加入

CC2538建立了网络  状态变化2-》8-》9  已经建立网络

麻烦看看哪里有问题?还是两个历程根本无法通讯?

  • zigbee2.5.1不行,HA1.2及以上的可以

    ZigBee 3.0的初始版本包括ZigBee智能家居(ZHA),ZigBee连接照明(ZLL),ZigBee楼宇自动化(ZBA),ZigBee零售服务(ZigBee Retail),ZigBee医疗保健(ZHC)和ZigBee电信服务。已经通过ZHA 1.2和ZLL 1.0认证的终端设备将向前兼容ZigBee 3.0标准,如果您正在开发基于ZHA 1.2或ZLL 1.0的产品,那您的产品将向前兼容ZigBee 3.0。
  • 建议版本一致