你好,CC2500的SO脚返回的数据,单片机读出来是0xFF,这个数据是错误的,应该是0x80,SO脚信号见下图:
调试程序见附件CC2500_test.rar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,CC2500的SO脚返回的数据,单片机读出来是0xFF,这个数据是错误的,应该是0x80,SO脚信号见下图:
调试程序见附件CC2500_test.rar
能否提供更详细的问题描述?是否测试过TI例程【
】?
TI 诚邀您参加全新设计的产品页面测试,参加测试即可享有 TI 购物 9 折优惠码,点击加入 EP产品页面测试报名,名额有限。感谢您的参与!
这个cc2500模块可能有问题,更换了一个模块,读出寄存器和ID的数据:
TI_CCxxx0_FIFOTHR initial_value:4
TI_CCxxx0_FIFOTHR:a
TI_CCxxx0_IOCFG2:0
TI_CCxxx0_IOCFG1:8
TI_CCxxx0_IOCFG0:f
TI_CCxxx0_IOCFG0:4
TI_CCxxx0_SYNC1:28
TI_CCxxx0_ADDR:2c
TI_CCxxx0_CHANNR:3c
TI_CCxxx0_FOCCFG:3c
read_id:d0
version:0
这个数据也不对吧?